Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: DRV10975
Hi All,
I am beginner of TI environment.
I develop an embedded system with motor control subsystem using "Tiva C Series TM4C1294 Connected LaunchPad Evaluation Kit".
Now I do a programming for I2C communication between the LaunchPad board and motor dirver board. I need information about a library for motor driver (DRV10975 12-V, Three-Phase, Sensorless BLDC Motor Driver). I got I2C.c and I2C.h file from site (TI Resource Explore), and use it for the communication. When I read document of "Using Feature Set of I2C Master on TM4C129x Microcontrollers", and used function SysCtlPeripheralReady for examples then I could not find where is the library including such the function. I think I have not yet installed necessary library.
There are so many documents, and I confused which document should I read firstly.
Best Regards,
Takano