This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS3137: CCS/TMS570LS3137:

Part Number: TMS570LS3137


Tool/software: Code Composer Studio

Hi,

This is Abhijith here, I am using Hercules development kit with controller TMS570LS3137 and CCS as an IDE , The development kit was working properly and i was trying to do EMIF communication to communicate with my synchronous DP RAM (i was using ASYNC 2 ) but it dint work .So i thought of working out with CS0 (ie with SRAM option) and programmed the board after that i am trying to program the board i am getting the following error

    

Error connecting to the target:
(Error -2062 @ 0x0)
Unable to halt device. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 6.0.579.0)

       The same program i tried in another board but the result is same , now both the boards are not taking the new program . I had only two boards with me both are not working. So it will be very helpful if you give solution for this.

Regards ,

Abhi