Part Number: TMS570LS1114
Hi,
The datasheet mentions AD1EVT can be set as GPIO. Which GPIO is it bound to? AD2EVT for example, is bound to GIOB[2].
Source: http://www.ti.com/lit/ug/spnu550b/spnu550b.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS1114
Hi,
The datasheet mentions AD1EVT can be set as GPIO. Which GPIO is it bound to? AD2EVT for example, is bound to GIOB[2].
Source: http://www.ti.com/lit/ug/spnu550b/spnu550b.pdf
Hi,
The TRM and datasheet say that AD1EVT can be configured as GPIO signal. When it is used as GPIO, it has the GPIO functionality:
1. Pull control feature: Pull-up or pull-down if enabled
2. Pin direction: input or output
3. Open-drain feature for output signal
It does not need to be tied to other GIO pin such as GIOB[2].
Regards,
QJ