Part Number: TM4C123GH6PZ
Tool/software: Code Composer Studio
Tiva bootloader
Hi I’ve develop board based on Tiva TM4C123GH6PZ. I’m communicating to this board via FDDI USB to UART converter chip. The FDDI chip is connected to TIVA UART0. When the TIva is erased I succeed to download firmware vis the UART using the LM Flash programmer. I add serial command in the s.w. that activate call to the ROM bootloader. When I try to download f.w. to TIVA I’m sending the command that call the BOOT Rom and that try to download a firmware via the LM flash program but I receive an error message. I’m using an IAR development environment. I’ve tried this scenario via code composer complier but I encounter the same problem. Does anyone has an Idea? Recommendation?
Thanks
Shmuel