This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART7 on Tiva C EK-TM4C1294XL LaunchPad



Hi All ,

I am using Tiva C series TM4C1294 Launchpad and i want to test the UART communication between the board and my laptop.

At first , the communication b/w my laptop and UART 0 of the TM4C1294 Launchpad has been tested and its working fine.

All i want is do is to test UART7 that has been brought out in the booster pack 1 ,which is not happening at this moment.

I will share the code that i used to check UART7 .

Please let me know any changes needs to be done in the code 


****************************************************************************

#include <stdint.h>
#include <stdbool.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "driverlib/debug.h"
#include "driverlib/gpio.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/rom.h"
#include "driverlib/rom_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"

//*****************************************************************************
//
//! \addtogroup example_list
//! <h1>UART Echo (uart_echo)</h1>
//!
//! This example application utilizes the UART to echo text. The first UART
//! (connected to the USB debug virtual serial port on the evaluation board)
//! will be configured in 115,200 baud, 8-n-1 mode. All characters received on
//! the UART are transmitted back to the UART.
//
//*****************************************************************************

//****************************************************************************
//
// System clock rate in Hz.
//
//****************************************************************************
uint32_t g_ui32SysClock;

//*****************************************************************************
//
// The error routine that is called if the driver library encounters an error.
//
//*****************************************************************************
#ifdef DEBUG
void
__error__(char *pcFilename, uint32_t ui32Line)
{
}
#endif

//*****************************************************************************
//
// The UART interrupt handler.
//
//*****************************************************************************
void
UARTIntHandler(void)
{
uint32_t ui32Status;

//
// Get the interrrupt status.
//
ui32Status = ROM_UARTIntStatus(UART7_BASE, true);

//
// Clear the asserted interrupts.
//
ROM_UARTIntClear(UART7_BASE, ui32Status);

//
// Loop while there are characters in the receive FIFO.
//
while(ROM_UARTCharsAvail(UART7_BASE))
{
//
// Read the next character from the UART and write it back to the UART.
//
ROM_UARTCharPutNonBlocking(UART7_BASE,
ROM_UARTCharGetNonBlocking(UART7_BASE));

//
// Blink the LED to show a character transfer is occuring.
//
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, GPIO_PIN_0);

//
// Delay for 1 millisecond. Each SysCtlDelay is about 3 clocks.
//
SysCtlDelay(g_ui32SysClock / (1000 * 3));

//
// Turn off the LED
//
GPIOPinWrite(GPIO_PORTN_BASE, GPIO_PIN_0, 0);
}
}

//*****************************************************************************
//
// Send a string to the UART.
//
//*****************************************************************************
void
UARTSend(const uint8_t *pui8Buffer, uint32_t ui32Count)
{
//
// Loop while there are more characters to send.
//
while(ui32Count--)
{
//
// Write the next character to the UART.
//
ROM_UARTCharPutNonBlocking(UART7_BASE, *pui8Buffer++);
}
}

//*****************************************************************************
//
// This example demonstrates how to send a string of data to the UART.
//
//*****************************************************************************
int
main(void)
{
//
// Set the clocking to run directly from the crystal at 120MHz.
//
g_ui32SysClock = MAP_SysCtlClockFreqSet((SYSCTL_XTAL_25MHZ |
SYSCTL_OSC_MAIN |
SYSCTL_USE_PLL |
SYSCTL_CFG_VCO_480), 120000000);
//
// Enable the GPIO port that is used for the on-board LED.
//
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPION);

//
// Enable the GPIO pins for the LED (PN0).
//
ROM_GPIOPinTypeGPIOOutput(GPIO_PORTN_BASE, GPIO_PIN_0);

//
// Enable the peripherals used by this example.
//

ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC);
ROM_SysCtlPeripheralEnable(SYSCTL_PERIPH_UART7);

//
// Enable processor interrupts.
//
ROM_IntMasterEnable();

//
// Set GPIO A0 and A1 as UART pins.
//
ROM_GPIOPinConfigure(GPIO_PC4_U7RX);
ROM_GPIOPinConfigure(GPIO_PC5_U7TX);
ROM_GPIOPinTypeUART(GPIO_PORTC_BASE,GPIO_PIN_4 |GPIO_PIN_5);

//UARTStdioConfig(7, 115200, g_ui32SysClock);

//
// Configure the UART for 115,200, 8-N-1 operation.
//
ROM_UARTConfigSetExpClk(UART7_BASE, g_ui32SysClock, 115200,
(UART_CONFIG_WLEN_8 | UART_CONFIG_STOP_ONE |
UART_CONFIG_PAR_NONE));
// UARTStdioConfig(7, 115200, g_ui32SysClock);

// Enable the UART interrupt.
//
ROM_IntEnable(INT_UART7);
ROM_UARTIntEnable(UART7_BASE, UART_INT_RX | UART_INT_RT);

//
// Prompt for text to be entered.
//
UARTSend((uint8_t *)"\033[2JEnter text: ", 16);

//
// Loop forever echoing data through the UART.
//
while(1)
{
}
}

Thanks,

Chandan

  • I did not see anything obvious in the code. How did you interface (what hardware did you use) to connect pins PC4 and PC5 to your computer? Perhaps you can attach a schematic of your connections to the RS2323 driver chip and the connections from that to the serial port on your PC (or USB to serial cable).
  • I second Bob, and suspect you are trying to connect TTL level communication directly to RS232 level comm on your PC/Adapter...