Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: EK-TM4C123GXL
Tool/software: Code Composer Studio
I am using timer interrupt .sending and receiving data through SPI and also using SSI interrupt but its not working
her is my code
#include <stdint.h>
#include <stdbool.h>
#include <math.h>
#include <stdio.h>
#include <stdlib.h>
//#include "inc/tm4c123gh6pm.h"
#include "inc/hw_memmap.h"
#include "inc/hw_ssi.h"
#include "inc/hw_ints.h"
#include "inc/hw_types.h"
#include "driverlib/ssi.h"
#include "driverlib/gpio.h"
#include "driverlib/pin_map.h"
#include "driverlib/interrupt.h"
#include "driverlib/sysctl.h"
#include "driverlib/timer.h"
SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI0);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOF);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOD);
SysCtlPeripheralEnable(SYSCTL_PERIPH_SSI1);
GPIOPinTypeGPIOOutput(GPIO_PORTB_BASE,GPIO_PIN_1);
GPIOPadConfigSet(GPIO_PORTB_BASE,GPIO_PIN_1,GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
GPIOPinConfigure(GPIO_PA2_SSI0CLK);
GPIOPinConfigure(GPIO_PA3_SSI0FSS);
GPIOPinConfigure(GPIO_PA5_SSI0TX);
GPIOPinConfigure(GPIO_PA4_SSI0RX);
GPIOPinTypeSSI(GPIO_PORTA_BASE,GPIO_PIN_5|GPIO_PIN_4|GPIO_PIN_3|GPIO_PIN_2);
// Wait for the SSI0 module to be ready.
//
//
// Configure the SSI.
//
SSIConfigSetExpClk(SSI0_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0, SSI_MODE_MASTER, 100000, 16);
//
//
// Enable the SSI module.
//
SSIEnable(SSI0_BASE);
// Enable the SSI module.
GPIOPinConfigure(GPIO_PD0_SSI1CLK);
GPIOPinConfigure(GPIO_PD1_SSI1FSS);
GPIOPinConfigure(GPIO_PD2_SSI1RX);
GPIOPinConfigure(GPIO_PD3_SSI1TX);
GPIOPinTypeSSI(GPIO_PORTD_BASE,GPIO_PIN_3|GPIO_PIN_2|GPIO_PIN_1|GPIO_PIN_0);
// Wait for the SSI0 module to be ready.
//
//
// Configure the SSI.
//
SSIConfigSetExpClk(SSI1_BASE, SysCtlClockGet(), SSI_FRF_MOTO_MODE_0, SSI_MODE_SLAVE, 100000, 16);
//
SSIEnable(SSI1_BASE);
//_________________Enable Timer_________________
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
TimerConfigure(TIMER0_BASE, TIMER_CFG_PERIODIC);
ui32Period = (SysCtlClockGet() / 10) / 2;
TimerLoadSet(TIMER0_BASE, TIMER_A, ui32Period -1);
IntEnable(INT_TIMER0A);
TimerIntEnable(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
IntMasterEnable();
TimerEnable(TIMER0_BASE, TIMER_A);
SSIIntEnable(SSI1_BASE, SSI_RXFF);
IntEnable(INT_SSI1);
while(1)
{
while(flag==0){};
flag=0;
uint32_t value;
value=0x00000000;
//send msg
SSIDataPut(SSI0_BASE,value);
while(SSIBusy(SSI0_BASE))
{
}
}
void Timer0IntHandler(void)
{
TimerIntClear(TIMER0_BASE, TIMER_TIMA_TIMEOUT);
flag=1;
}
void SSI1IntHandler(void)
{
SSIDataGet(SSI1_BASE, &g_data);
GPIOPinWrite(GPIO_PORTB_BASE, GPIO_PIN_1,g_data);
//
// Clear interrupts.
//
SSIIntClear(SSI1_BASE,SSI_RXFF);
}