This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C123GXL: USB OTG Mouse Example - Hardware and Software Issues

Part Number: EK-TM4C123GXL

Hello,

I am working on a project to control a robotic arm with a USB Mouse/Keyboard, and my partner and I have been struggling for the past week trying to connect the USB Mouse to connect and power on through the USB Device Port built on the TM4C MCU.

So far, we have R25 and R29 shorted to enable the USB device to receive power and also shorted the two pins above R14 (center and right).

So far, when we plug the USB Mouse into the board, it flashes the red LED on for a split second, then turns off and stays off. But the PWR LED on the board still stays on, so the board is still receiving power from the USB Port.

We used the example from "C:\ti\TivaWare_C_Series-2.1.3.156\usb_otg_mouse" and are trying to make it work with the EK-TM4C123GXL board.

If anyone has any suggestions on how we are wiring it and if there are any examples that work with our particular board, please let us know! Also, if there are any licensing issues since we are using the free software trial, please let us know if this is possible and if we should continue or not.

This is our current system overview:

Thanks in advance!

Sheldon