Part Number: TMDXRM46HDK
Other Parts Discussed in Thread: RM46L852
Tool/software: Code Composer Studio
Hello,
On our Hercules RM46x Development Kit, we would like to map some memory sections to external memory. However, doing just that with the linker command file results in the following GEL error:
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
CortexR4: File Loader: Verification failed: Values at address 0x80000020 do not match Please verify target memory and memory map.
CortexR4: GEL: File: /local_ssd2/tmp/WIP/LaunchProj0_RM46/Release/LaunchProj0_RM46.out: a data verification error occurred, file load failed.
CortexR4: GEL Output: Memory Map Setup for Flash @ Address 0x0 due to System Reset
In CCS, the connection is to "RM46L852" via the "Texas Instruments XDS100v2 USB Debug Probe".
The gel file is emulation/gel/rm46l852.gel
The sections ar defined as follows:
MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000040 length=0x0017FFC0
FLASH1 (RX) : origin=0x00180000 length=0x00180000
STACKS (RW) : origin=0x08000000 length=0x00004500
RAM (RW) : origin=0x08004500 length=0x0002BB00
RAM_EXT (RW) : origin=0x80000000 length=0x00800000
}
SECTIONS
{
.intvecs : {} > VECTORS
.text : {} > RAM_EXT
.const : {} > RAM_EXT
.cinit : {} > RAM_EXT
.pinit : {} > RAM_EXT
.bss : {} > RAM_EXT
.data : {} > RAM_EXT
.sysmem : {} > RAM_EXT
.stack : {} > RAM_EXT
.ARM.extab: {} > RAM_EXT
.ARM.exidx: {} > RAM_EXT
}
The linker options are:
-mv7R4 --code_state=32 --float_support=fpalib -me -O3 --symdebug:none --diag_warning=225 --diag_wrap=off --display_error_number --enum_type=int --wchar_t=32 --abi=eabi -z -m"LaunchProj0_RM46.map" -i"/local_hdd/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.1.LTS/lib" -i"/local_hdd/ti/ccsv7/tools/compiler/ti-cgt-arm_16.9.1.LTS/include" --reread_libs --diag_wrap=off --display_error_number --warn_sections --xml_link_info="LaunchProj0_RM46_linkInfo.xml" --trampolines=on -o "LaunchProj0_RM46.out" "./source/main.obj" "/local_ssd2/tmp/WIP/rm46hdk.cmd" -lrtsv7R4_A_le_eabi.lib
I guess I'm missing something but I don't see what - any help is highy appreciated.