Other Parts Discussed in Thread: RM46L852
Hi,
I know the Error Pin of the TMS/RM series are triggered by the internal lockstep architecture. However, is there a way to use the same pin to signal a software code error?
I'm designing a Dual Modular Redundant flight controller as active/passive architecture using the RM46L852 and the TPS65381. The Error pin should trigger the TPS65381 and use its DRVENABLE pin to toggle a arbiter logic. But this should happen even as a lockstep HW error and as a software error (manually triggered, e.g. IMU sensor inconsistency values).
Any suggestions?
Can I also share the MCU Error pin with other logics?
How can I drive a Error-LED using the Error Pin?
Is there also a way to reset external the TPS65381 to force a complete power cycle?
Thanks,
-Jarno