Part Number: EK-TM4C1294XL
Hi,
I try to build enet_io example on CCS, but setting up has issue (open project -> build project is not work).
So, I make new project and copy files to the project, then I meet linking error, I do not know which file must be included into the project.
There is no file dependency list so I search file with text search software belonging to error message. This takes time for searches and try to set up.
If possible please consider to make dependency list to build example projects.
I meet linking error as follows;
<Linking>
undefined first referenced
symbol in file
--------- ----------------
DecodeFormString ./main.obj
FindCGIParameter ./main.obj
GetCGIParam ./main.obj
LocatorAppTitleSet ./main.obj
LocatorInit ./main.obj
LocatorMACAddrSet ./main.obj
PinoutSet ./main.obj
UARTStdioConfig ./main.obj
UARTprintf ./main.obj
http_set_cgi_handlers ./main.obj
http_set_ssi_handler ./main.obj
httpd_init ./main.obj
io_get_animation_speed ./main.obj
io_get_animation_speed_string ./main.obj
io_get_ledstate ./main.obj
io_init ./main.obj
io_is_led_on ./main.obj
io_set_animation_speed ./main.obj
io_set_led ./main.obj
lwIPInit ./main.obj
lwIPLocalIPAddrGet ./main.obj
lwIPTimer ./main.obj
usnprintf ./main.obj
usprintf ./main.obj
error #10234-D: unresolved symbols remain
Which files must be included or how to set link for it?
Best Regards,
S.Takano