Other Parts Discussed in Thread: EK-LM3S3748, LM3S3748
Hi,
I'm using EVB-LM3S3748, and would like to operate a boot loader using UART.
I've read the user guide: SW-BOOTLDR-UG-6075.pdf.
I did the following:
1) Modified file bl_config.h in example boot_usb to support UART rather the original USB (pasted below).
2) Modified the example usb_boot_demo2 the following way:
- Eliminated all LCD/graphic related code.
- Initialized both UART0 and UART1 (I have them both wired to an extension board for RS232 connection. JP12 & JP25 are cut)
- Replaced the 'wait for select button' code with a simple countdown loop which waits ~1Sec.
- (*((void (*)(void))(*(unsigned long *)0x2c)))(); is performed after wait loop is over.
3) Connected with LM Flash Programmer (build 1089) in ICDI (EVAL Board mode).
4) Erased entire flash under "Flash Utilities" tab.
5) Loaded 'serial_flash_loader.bin' under "Program" tab (in order to mimic a brand new device).
6) Used sflash.exe (compiled from the sources in 6075) to program the device as follows:
sflash usb_boot_demo2.bin -p 0x1800 -l boot_usb.bin -c 3
The result is that the demo program IS running (I can see the prints on the terminal. prints are only from UART1), however, the next attempts to program the device using the command line fail (does not sync with device). I used the following command line:
sflash usb_boot_demo2.bin -p 0x1800 -c 3
I've also tried to eliminate baud rate detection (-d) with no success.
Repeating steps 3..6, but with separate loads for 'boot_usb.bin' (to 0x0000) and 'usb_boot_demo2.bin' (to 0x1800) had similar result.
My compiler is IAR Embedded Workbench 5.5 .
What am I missing here?
Thanks for your help,
Asaf.
| //***************************************************************************** // // bl_config.h - The configurable parameters of the boot loader. // // Copyright (c) 2008-2010 Texas Instruments Incorporated. All rights reserved. // Software License Agreement // // Texas Instruments (TI) is supplying this software for use solely and // exclusively on TI's microcontroller products. The software is owned by // TI and/or its suppliers, and is protected under applicable copyright // laws. You may not combine this software with "viral" open-source // software in order to form a larger program. // // THIS SOFTWARE IS PROVIDED "AS IS" AND WITH ALL FAULTS. // NO WARRANTIES, WHETHER EXPRESS, IMPLIED OR STATUTORY, INCLUDING, BUT // NOT LIMITED TO, IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR // A PARTICULAR PURPOSE APPLY TO THIS SOFTWARE. TI SHALL NOT, UNDER ANY // CIRCUMSTANCES, BE LIABLE FOR SPECIAL, INCIDENTAL, OR CONSEQUENTIAL // DAMAGES, FOR ANY REASON WHATSOEVER. // // This is part of revision 6075 of the EK-LM3S3748 Firmware Package. // //***************************************************************************** #ifndef __BL_CONFIG_H__ #define __BL_CONFIG_H__ //***************************************************************************** // // The following defines are used to configure the operation of the boot // loader. For each define, its interactions with other defines are described. // First is the dependencies (in other words, the defines that must also be // defined if it is defined), next are the exclusives (in other words, the // defines that can not be defined if it is defined), and finally are the // requirements (in other words, the defines that must be defined if it is // defined). // // The following defines must be defined in order for the boot loader to // operate: // // One of CAN_ENABLE_UPDATE, ENET_ENABLE_UPDATE, I2C_ENABLE_UPDATE, // SSI_ENABLE_UPDATE, UART_ENABLE_UPDATE, or USB_ENABLE_UPDATE // APP_START_ADDRESS // VTABLE_START_ADDRESS // FLASH_PAGE_SIZE // STACK_SIZE // //***************************************************************************** //***************************************************************************** // // The frequency of the crystal used to clock the microcontroller. // // This defines the crystal frequency used by the microcontroller running the // boot loader. If this is unknown at the time of production, then use the // UART_AUTOBAUD feature to properly configure the UART. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define CRYSTAL_FREQ 8000000 //***************************************************************************** // // This enables the boosting of the LDO voltage to 2.75V. For boot loader // configurations that enable the PLL (for example, using the Ethernet port) // on a part that has the PLL errata, this should be enabled. This applies to // revision A2 of Fury-class devices. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define BOOST_LDO_VOLTAGE //***************************************************************************** // // The starting address of the application. This must be a multiple of 1024 // bytes (making it aligned to a page boundary). A vector table is expected at // this location, and the perceived validity of the vector table (stack located // in SRAM, reset vector located in flash) is used as an indication of the // validity of the application image. // // The flash image of the boot loader must not be larger than this value. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define APP_START_ADDRESS 0x1800 //***************************************************************************** // // The address at which the application locates its exception vector table. // This must be a multiple of 1024 bytes (making it aligned to a page // boundary). Typically, an application will start with its vector table and // this value should be set to APP_START_ADDRESS. This option is provided to // cater for applications which run from external memory which may not be // accessible by the NVIC (the vector table offset register is only 30 bits // long). // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define VTABLE_START_ADDRESS 0x1800 //***************************************************************************** // // The size of a single, erasable page in the flash. This must be a power // of 2. The default value of 1024 bytes represents the page size for the // internal flash on all Stellaris MCUs and this value should only be // overridden if configuring a boot loader to access external flash devices // with a page size different from this. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define FLASH_PAGE_SIZE 0x00000400 //***************************************************************************** // // The amount of space at the end of flash to reserved. This must be a // multiple of 1024 bytes (making it aligned to a page boundary). This // reserved space is not erased when the application is updated, providing // non-volatile storage that can be used for parameters. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define FLASH_RSVD_SPACE 0x00000800 //***************************************************************************** // // The number of words of stack space to reserve for the boot loader. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define STACK_SIZE 128 //***************************************************************************** // // The number of words in the data buffer used for receiving packets. This // value must be at least 3. If using auto-baud on the UART, this must be at // least 20. The maximum usable value is 65 (larger values will result in // unused space in the buffer). // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** #define BUFFER_SIZE 20 //***************************************************************************** // // Enables updates to the boot loader. Updating the boot loader is an unsafe // operation since it is not fully fault tolerant (losing power to the device // part way though could result in the boot loader no longer being present in // flash). // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENABLE_BL_UPDATE //***************************************************************************** // // This definition will cause the the boot loader to erase the entire flash on // updates to the boot loader or to erase the entire application area when the // application is updated. This erases any unused sections in the flash before // the firmware is updated. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define FLASH_CODE_PROTECTION //***************************************************************************** // // Enables the call to decrypt the downloaded data before writing it into // flash. The decryption routine is empty in the reference boot loader source, // which simply provides a placeholder for adding an actual decryption // algorithm. Although this option is retained for backwards compatibility, it // is recommended that a decryption function be specified using the newer hook // function mechanism and BL_DECRYPT_FN_HOOK instead. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENABLE_DECRYPTION //***************************************************************************** // // Enables support for the MOSCFAIL handler in the NMI interrupt. // Note: Sandstorm or Fury devices do not provide the MOSCFAIL reset, so this // feature should not be enabled for these devices. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENABLE_MOSCFAIL_HANDLER //***************************************************************************** // // Enables support for the code to be compatible with the flash patch that is // preloaded into the flash of certain Stellaris devices. This support should // only be enabled for devices that require it. // // Note: Enabling this feature will cause the boot loader to expect to be // loaded at 0x1000, despite the fact that debuggers will still think that it // should be loaded at 0x0. Therefore, LM Flash Programmer must be used to // program the boot loader into flash when using this feature. // // Depends on: None // Exclusive of: None // Requires: None // //***************************************************************************** //#define FLASH_PATCH_COMPATIBLE //***************************************************************************** // // Enables the pin-based forced update check. When enabled, the boot loader // will go into update mode instead of calling the application if a pin is read // at a particular polarity, forcing an update operation. In either case, the // application is still able to return control to the boot loader in order to // start an update. For applications which need to perform more complex // checking than is possible using a single GPIO, a hook function may be // provided using BL_CHECK_UPDATE_FN_HOOK instead. // // Depends on: None // Exclusive of: None // Requires: FORCED_UPDATE_PERIPH, FORCED_UPDATE_PORT, FORCED_UPDATE_PIN, // FORCED_UPDATE_POLARITY // //***************************************************************************** //#define ENABLE_UPDATE_CHECK //***************************************************************************** // // The GPIO module to enable in order to check for a forced update. This will // be one of the SYSCTL_RCGC2_GPIOx values, where "x" is replaced with the port // name (such as B). The value of "x" should match the value of "x" for // FORCED_UPDATE_PORT. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** //#define FORCED_UPDATE_PERIPH SYSCTL_RCGC2_GPIOB //***************************************************************************** // // The GPIO port to check for a forced update. This will be one of the // GPIO_PORTx_BASE values, where "x" is replaced with the port name (such as // B). The value of "x" should match the value of "x" for // FORCED_UPDATE_PERIPH. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** //#define FORCED_UPDATE_PORT GPIO_PORTB_BASE //***************************************************************************** // // The pin to check for a forced update. This is a value between 0 and 7. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** //#define FORCED_UPDATE_PIN 7 //***************************************************************************** // // The polarity of the GPIO pin that results in a forced update. This value // should be 0 if the pin should be low and 1 if the pin should be high. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** //#define FORCED_UPDATE_POLARITY 0 //***************************************************************************** // // This enables a weak pull-up or pull-down for the GPIO pin used in a forced // update. Only one of FORCED_UPDATE_WPU or FORCED_UPDATE_WPD should be // defined, or neither if a weak pull-up or pull-down is not required. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** //#define FORCED_UPDATE_WPU //#define FORCED_UPDATE_WPD //***************************************************************************** // // This enables the use of the GPIO_LOCK mechanism for configuration of // protected GPIO pins (for example JTAG pins). If this value is not defined, // the locking mechanism will not be used. The only legal values for this // feature are GPIO_LOCK_KEY for Fury devices and GPIO_LOCK_KEY_DD for all // other devices except Sandstorm devices, which do not support this feature. // // Depends on: ENABLE_UPDATE_CHECK // Exclusive of: None // Requries: None // //***************************************************************************** //#define FORCED_UPDATE_KEY GPIO_LOCK_KEY //#define FORCED_UPDATE_KEY GPIO_LOCK_KEY_DD //***************************************************************************** // // Selects the UART as the port for communicating with the boot loader. // // Depends on: None // Exclusive of: CAN_ENABLE_UPDATE, ENET_ENABLE_UPDATE, I2C_ENABLE_UPDATE, // SSI_ENABLE_UPDATE, USB_ENABLE_UPDATE // Requires: UART_AUTOBAUD or UART_FIXED_BAUDRATE, BUFFER_SIZE // //***************************************************************************** #define UART_ENABLE_UPDATE //***************************************************************************** // // Enables automatic baud rate detection. This can be used if the crystal // frequency is unknown, or if operation at different baud rates is desired. // // Depends on: UART_ENABLE_UPDATE // Exclusive of: UART_FIXED_BAUDRATE // Requires: None // //***************************************************************************** #define UART_AUTOBAUD //***************************************************************************** // // Selects the baud rate to be used for the UART. // // Depends on: UART_ENABLE_UPDATE, CRYSTAL_FREQ // Exclusive of: UART_AUTOBAUD // Requires: None // //***************************************************************************** //#define UART_FIXED_BAUDRATE 115200 //***************************************************************************** // // Selects the SSI port as the port for communicating with the boot loader. // // Depends on: None // Exclusive of: CAN_ENABLE_UPDATE, ENET_ENABLE_UPDATE, I2C_ENABLE_UPDATE, // UART_ENABLE_UPDATE, USB_ENABLE_UPDATE // Requires: BUFFER_SIZE // //***************************************************************************** //#define SSI_ENABLE_UPDATE //***************************************************************************** // // Selects the I2C port as the port for communicating with the boot loader. // // Depends on: None // Exclusive of: CAN_ENABLE_UPDATE, ENET_ENABLE_UPDATE, SSI_ENABLE_UPDATE, // UART_ENABLE_UPDATE, USB_ENABLE_UPDATE // Requires: I2C_SLAVE_ADDR, BUFFER_SIZE // //***************************************************************************** //#define I2C_ENABLE_UPDATE //***************************************************************************** // // Specifies the I2C address of the boot loader. // // Depends on: I2C_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define I2C_SLAVE_ADDR 0x42 //***************************************************************************** // // Selects Ethernet update via the BOOTP/TFTP protocol. // // Depends on: None // Exclusive of: CAN_ENABLE_UPDATE, I2C_ENABLE_UPDATE, SSI_ENABLE_UPDATE, // UART_ENABLE_UPDATE, USB_ENABLE_UPDATE // Requires: CRYSTAL_FREQ // //***************************************************************************** //#define ENET_ENABLE_UPDATE //***************************************************************************** // // Enables the use of the Ethernet status LED outputs to indicate traffic and // connection status. // // Depends on: ENET_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENET_ENABLE_LEDS //***************************************************************************** // // Specifies the hard coded MAC address for the Ethernet interface. There are // six individual values (ENET_MAC_ADDR0 through ENET_MAC_ADDR5) that provide // the six bytes of the MAC address, where ENET_MAC_ADDR0 though ENET_MAC_ADDR2 // provide the organizationally unique identifier (OUI) and ENET_MAC_ADDR3 // through ENET_MAC_ADDR5 provide the extension identifier. If these values // are not provided, the MAC address will be extracted from the user registers. // // Depends on: ENET_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENET_MAC_ADDR0 0x00 //#define ENET_MAC_ADDR1 0x00 //#define ENET_MAC_ADDR2 0x00 //#define ENET_MAC_ADDR3 0x00 //#define ENET_MAC_ADDR4 0x00 //#define ENET_MAC_ADDR5 0x00 //***************************************************************************** // // Specifies the name of the BOOTP server from which to request information. // The use of this specifier allows a board-specific BOOTP server to co-exist // on a network with the DHCP server that may be part of the network // infrastructure. The BOOTP server provided by Texas Instruments requires // that this be set to "stellaris". // // Depends on: ENET_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define ENET_BOOTP_SERVER "stellaris" //***************************************************************************** // // Selects USB update via Device Firmware Update class. // // Depends on: None // Exclusive of: CAN_ENABLE_UPDATE, ENET_ENABLE_UPDATE, I2C_ENABLE_UPDATE, // SSI_ENABLE_UPDATE, UART_ENABLE_UPDATE, // Requires: CRYSTAL_FREQ, USB_VENDOR_ID, USB_PRODUCT_ID, USB_DEVICE_ID, // USB_MAX_POWER // //***************************************************************************** //#define USB_ENABLE_UPDATE //***************************************************************************** // // The USB vendor ID published by the DFU device. This value is the TI // Stellaris vendor ID. Change this to the vendor ID you have been assigned by // the USB-IF. // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_VENDOR_ID 0x1cbe //***************************************************************************** // // The USB device ID published by the DFU device. If you are using your own // vendor ID, chose a device ID that is different from the ID you use in // non-update operation. If you have sublicensed TI's vendor ID, you must // use an assigned product ID here. // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_PRODUCT_ID 0x00FF //***************************************************************************** // // Selects the BCD USB device release number published in the device // descriptor. // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_DEVICE_ID 0x0001 //***************************************************************************** // // Sets the maximum power consumption that the DFU device will report to the // USB host in the configuration descriptor. Units are milliamps. // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_MAX_POWER 150 //***************************************************************************** // // Specifies whether the DFU device reports to the host that it is self-powered // (defined as 0) or bus-powered (defined as 1). // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_BUS_POWERED 1 //***************************************************************************** // // Specifies whether the target board uses a multiplexer to select between USB // host and device modes. // // Depends on: USB_ENABLE_UPDATE // Exclusive of: None // Requires: USB_MUX_PERIPH, USB_MUX_PORT, USB_MUX_PIN, USB_MUX_DEVICE // //***************************************************************************** //#define USB_HAS_MUX //***************************************************************************** // // Specifies the GPIO peripheral containing the pin which is used to select // between USB host and device modes. The value is of the form // SYSCTL_PERIPH_GPIOx, where GPIOx represents the required GPIO port. // // Depends on: USB_ENABLE_UPDATE, USB_HAS_MUX // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_MUX_PERIPH SYSCTL_RCGC2_GPIOH //***************************************************************************** // // Specifies the GPIO port containing the pin which is used to select between // USB host and device modes. The value is of the form GPIO_PORTx_BASE, where // PORTx represents the required GPIO port. // // Depends on: USB_ENABLE_UPDATE, USB_HAS_MUX // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_MUX_PORT GPIO_PORTH_BASE //***************************************************************************** // // Specifies the GPIO pin number used to select between USB host and device // modes. Valid values are 0 through 7. // // Depends on: USB_ENABLE_UPDATE, USB_HAS_MUX // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_MUX_PIN 2 //***************************************************************************** // // Specifies the state of the GPIO pin required to select USB device-mode // operation. Valid values are 0 (low) or 1 (high). // // Depends on: USB_ENABLE_UPDATE, USB_HAS_MUX // Exclusive of: None // Requires: None // //***************************************************************************** //#define USB_MUX_DEVICE 1 //***************************************************************************** // // Selects an update via the CAN port. // // Depends on: None // Exclusive of: ENET_ENABLE_UPDATE, I2C_ENABLE_UPDATE, SSI_ENABLE_UPDATE, // UART_ENABLE_UPDATE, USB_ENABLE_UPDATE // Requires: CAN_RX_PERIPH, CAN_RX_PORT, CAN_RX_PIN, CAN_TX_PERIPH, // CAN_TX_PORT, CAN_TX_PIN, CAN_BIT_RATE, CRYSTAL_FREQ. // //***************************************************************************** //#define CAN_ENABLE_UPDATE //***************************************************************************** // // Enables the UART to CAN bridging for use when the CAN port is selected for // communicating with the boot loader. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_UART_BRIDGE //***************************************************************************** // // The GPIO module to enable in order to configure the CAN0 Rx pin. This will // be one of the SYSCTL_RCGC2_GPIOx values, where "x" is replaced with the port // name (such as B). The value of "x" should match the value of "x" for // CAN_RX_PORT. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_RX_PERIPH SYSCTL_RCGC2_GPIOA //***************************************************************************** // // The GPIO port used to configure the CAN0 Rx pin. This will be one of the // GPIO_PORTx_BASE values, where "x" is replaced with the port name (such as // B). The value of "x" should match the value of "x" for CAN_RX_PERIPH. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_RX_PORT GPIO_PORTA_BASE //***************************************************************************** // // The GPIO pin that is shared with the CAN0 Rx pin. This is a value between 0 // and 7. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_RX_PIN 4 //***************************************************************************** // // The GPIO module to enable in order to configure the CAN0 Tx pin. This will // be one of the SYSCTL_RCGC2_GPIOx values, where "x" is replaced with the port // name (such as B). The value of "x" should match the value of "x" for // CAN_TX_PORT. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_TX_PERIPH SYSCTL_RCGC2_GPIOA //***************************************************************************** // // The GPIO port used to configure the CAN0 Tx pin. This will be one of the // GPIO_PORTx_BASE values, where "x" is replaced with the port name (such as // B). The value of "x" should match the value of "x" for CAN_TX_PERIPH. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_TX_PORT GPIO_PORTA_BASE //***************************************************************************** // // The GPIO pin that is shared with the CAN0 Tx pin. This is a value between 0 // and 7. // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_TX_PIN 5 //***************************************************************************** // // The bit rate used on the CAN bus. This must be one of 20000, 50000, 125000, // 250000, 500000, or 1000000. The CAN bit rate must be less than or equal to // the crystal frequency divided by 8 (CRYSTAL_FREQ / 8). // // Depends on: CAN_ENABLE_UPDATE // Exclusive of: None // Requires: None // //***************************************************************************** //#define CAN_BIT_RATE 1000000 //***************************************************************************** // // Performs application-specific low level hardware initialization on system // reset. If hooked, this function will be called immediately after the boot // loader code relocation completes. An application may perform any required // low-level hardware initialization during this function. Note that the // system clock has not been set when this function is called. Initialization // that assumes the system clock is set may be performed in the BL_INIT_FN_HOOK // function instead. // // void MyHwInitFunc(void); // //***************************************************************************** //#define BL_HW_INIT_FN_HOOK MyHwInitFunc //***************************************************************************** // // Performs application-specific initialization on system reset. If hooked, // this function will be called during boot loader initialization to perform // any board- or application-specific initialization which is required. The // function is called following a reset immediately after the selected boot // loader peripheral has been configured and the system clock has been set. // // void MyInitFunc(void); // //***************************************************************************** //#define BL_INIT_FN_HOOK MyInitFunc //***************************************************************************** // // Performs application-specific reinitialization on boot loader entry via SVC. // If hooked, this function will be called during boot loader reinitialization // to perform any board- or application-specific initialization which is // required. The function is called following boot loader entry from an // application, after any system clock rate adjustments have been made. // // void MyReinitFunc(void); // //***************************************************************************** //#define BL_REINIT_FN_HOOK MyReinitFunc //***************************************************************************** // // Informs an application that a download is starting. If hooked, this // function will be called when a firmware download is about to begin. The // function is called after the first data packet of the download is received // but before it has been written to flash. // // void MyStartFunc(void); // //***************************************************************************** //#define BL_START_FN_HOOK MyStartFunc //***************************************************************************** // // Informs an application of download progress. If hooked, this function will // be called periodically during a firmware download to provide progress // information. The function is called after each data packet is received from // the host. Parameters provide the number of bytes of data received and, in // cases other than Ethernet update, the expected total number of bytes in the // download (the TFTP protocol used by the Ethernet boot loader does not send // the final image size before the download starts so in this case the ulTotal // parameter is set to 0 to indicate that the size is unknown). // // void MyProgressFunc(unsigned long ulCompleted, unsigned long ulTotal); // //***************************************************************************** //#define BL_PROGRESS_FN_HOOK MyProgressFunc //***************************************************************************** // // Informs an application that a download has completed. If hooked, this // function will be called when a firmware download has just completed. The // function is called after the final data packet of the download has been // written to flash. // // void MyEndFunc(void); // //***************************************************************************** //#define BL_END_FN_HOOK MyEndFunc //***************************************************************************** // // Allows an application to perform in-place data decryption during download. // If hooked, this function will be called to perform in-place decryption of // each data packet received during a firmware download. // // void MyDecryptionFunc(unsigned char *pucBuffer, unsigned long ulSize); // // This value takes precedence over ENABLE_DECRYPTION. If both are defined, // the hook function defined using BL_DECRYPT_FN_HOOK is called rather than the // previously-defined DecryptData() stub function. // //***************************************************************************** //#define BL_DECRYPT_FN_HOOK MyDecryptionFunc //***************************************************************************** // // Allows an application to force a new firmware download. If hooked, this // function will be called during boot loader initialization to determine // whether a firmware update should be performed regardless of whether a valid // main code image is already present. If the function returns 0, the existing // main code image is booted (if present), otherwise the boot loader will wait // for a new firmware image to be downloaded. // // unsigned long MyCheckUpdateFunc(void); // // This value takes precedence over ENABLE_UPDATE_CHECK} if both are defined. // If you wish to perform a GPIO check in addition to any other update check // processing required, the GPIO code must be included within the hook function // itself. // //***************************************************************************** //#define BL_CHECK_UPDATE_FN_HOOK MyCheckUpdateFunc //***************************************************************************** // // Allows an application to replace the flash block erase function. If hooked, // this function will be called whenever a block of flash is to be erased. The // function must erase the block and wait until the operation has completed. // The size of the block which will be erased is defined by FLASH_BLOCK_SIZE. // // void MyFlashEraseFunc(unsigned long ulBlockAddr); // //***************************************************************************** //#define BL_FLASH_ERASE_FN_HOOK MyFlashEraseFunc //***************************************************************************** // // Allows an application to replace the flash programming function. If hooked, // this function will be called to program the flash with firmware image data // received during download operations. The function must program the supplied // data and wait until the operation has completed. // // void MyFlashProgramFunc(unsigned long ulDstAddr, // unsigned char *pucSrcData, // unsigned long ulLength); // //***************************************************************************** //#define BL_FLASH_PROGRAM_FN_HOOK MyFlashProgramFunc //***************************************************************************** // // Allows an application to replace the flash error clear function. If hooked, // this function must clear any flash error indicators and prepare to detect // access violations that may occur in a future erase or program operations. // // void MyFlashClearErrorFunc(void); // //***************************************************************************** //#define BL_FLASH_CL_ERR_FN_HOOK MyFlashClearErrorFunc //***************************************************************************** // // Reports whether or not a flash access violation error has occurred. If // hooked, this function will be called after flash erase or program // operations. The return code indicates whether or not an access violation // error occurred since the last call to the function defined by // BL_FLASH_CL_ERR_FN_HOOK, with 0 indicating no errors and non-zero indicating // an error. // // unsigned long MyFlashErrorFunc(void); // //***************************************************************************** //#define BL_FLASH_ERROR_FN_HOOK MyFlashErrorFunc //***************************************************************************** // // Reports the total size of the device flash. If hooked, this function will // be called to determine the size of the supported flash device. The return // code is the number of bytes of flash in the device. Note that this does not // take into account any reserved space defined via the FLASH_RSVD_SPACE value. // // unsigned long MyFlashSizeFunc(void); // //***************************************************************************** //#define BL_FLASH_SIZE_FN_HOOK MyFlashSizeFunc //***************************************************************************** // // Reports the address of the first byte after the end of the device flash. If // hooked, this function will be called to determine the address of the end of // valid flash. Note that this does not take into account any reserved space // defined via the FLASH_RSVD_SPACE value. // // unsigned long MyFlashEndFunc(void); // //***************************************************************************** //#define BL_FLASH_END_FN_HOOK MyFlashEndFunc //***************************************************************************** // // Checks whether the start address and size of an image are valid. If hooked, // this function will be called when a new firmware download is about to start. // Parameters provided are the requested start address for the new download // and, when using protocols which transmit the image length in advance, the // size of the image that is to be downloaded. The return code will be // non-zero to indicate that the start address is valid and the image will fit // in the available space, or 0 if either the address is invalid or the image // is too large for the device. // // unsigned long MyFlashAddrCheckFunc(unsigned long ulAddr, // unsigned long ulSize); // //***************************************************************************** //#define BL_FLASH_AD_CHECK_FN_HOOK MyFlashAddrCheckFunc #endif // __BL_CONFIG_H__ |
| int main(void) { unsigned long _delay = 4500000L; // // Set the clocking to run directly from the crystal. // ROM_SysCtlClockSet(SYSCTL_SYSDIV_1 | SYSCTL_USE_OSC | SYSCTL_OSC_MAIN | SYSCTL_XTAL_8MHZ); UARTStdioInit(1); // // Enable the UART peripheral for use. // SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA); SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOC); SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0); SysCtlPeripheralEnable(SYSCTL_PERIPH_UART1); // // Configure the UART for 115200, n, 8, 1 // UARTConfigSetExpClk(UART0_BASE, SysCtlClockGet(), 115200, (UART_CONFIG_PAR_NONE | UART_CONFIG_STOP_ONE | UART_CONFIG_WLEN_8)); // // Configure the UART for 115200, n, 8, 1 // UARTConfigSetExpClk(UART1_BASE, SysCtlClockGet(), 115200, (UART_CONFIG_PAR_NONE | UART_CONFIG_STOP_ONE | UART_CONFIG_WLEN_8)); GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1); GPIOPinTypeUART(GPIO_PORTC_BASE, GPIO_PIN_6 | GPIO_PIN_7); UARTprintf("Wait for BL jump..."); while (_delay--) { if (_delay < 100L) { UARTprintf("Go\r\n"); break; } } // // Call the boot loader so that it will listen for an update on the UART. // (*((void (*)(void))(*(unsigned long *)0x2c)))(); // // The boot loader should take control, so this should never be reached. // Just in case, loop forever. // while(1) { } } |