Part Number: TM4C1294NCPDT
Hi,
I would like to set TM4C1294 device to output SPI signal at 25MHz.
1. The level of MOSI is incorrect. Why? Is it required to add pullup resistor?
2. I was trying to set the SPI clock to 25MHz but the actual SPI clock will be 30MHz. If I set it to 20MHz, it will output 20MHz clock. It is weird when clock is over 20MHz.
https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/908/hello.7z
3. Is it possible to set either MISO or MOSI as open-drain? MISO and MOSI may be used at different voltage level.
Regards,
Edward