Part Number: TMS570LS0432
Hi,
I am using TMS 570Ls0432 in my design. I would like to know what is the maximum input voltage that I can give at the adv input pins of the device.
Thanks & best regards,
Veena Anns george
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS0432
Hi,
I am using TMS 570Ls0432 in my design. I would like to know what is the maximum input voltage that I can give at the adv input pins of the device.
Thanks & best regards,
Veena Anns george
Hello Veena,
There are really two voltages of concern when discussing maximum voltages. First is the absolute maximum voltage that can be applied without causing damage.
Make note of note 2 above as these absolute maximums should only be temporary as they can cause reduced reliability if present for long periods of time during use.
The second maximum voltage of concern is normal operating voltages. The maximum recommended voltage on an input is 3.6V (or Vccio+0.3V). If the input voltage is more than 0.3V higher than the VCCIO voltage, it can cause reverse biasing internal to the chip resulting in excessive leakage currents at the pin.
Dear Chuck Davenport,
Thanks for the detailed answer. The schematics of the ADC input is as shown in the figure. ( I have 1K resisor in the front of ADC)
If a fault in the analog front end circuit before the input pin in the figure above produces the voltage of 7 volts at I/P (i.e., more than maximum operating limit of micro controller), will it damage microcontroller?
Since i have 1 K resistor, the current is always 7mA . This is in the acceptable range. Please let me know your comment on this?
Thanks& Best regards,
Veena Anns George