This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Yes the dip switches as well as the "debug" switch on the Launch Pad were selected. Initially I had a hard time getting the Virtual Serial Port Loaded, however it now works whenever the Launch Pad is detected. I have been able to run simple blink app as well as Project O which is more complex, so I know I am communicating with the board. When I stack the pervasive extension board and the EPD I do not get a picture nor can the PDI app sees the port and the load "fails". Both the UniFlash and CCS are not in my frequently used tools so I am overwhelmed by the sequence of things you have to do and its entirely possible I went down an unaccepted path.
When I start a new project it has me ID my Launch Pad EK-TM4C123GXL ,
Auto select Stellaris ICDI as “Selected Connection”
Create Session from Existing Target Configuration file Tiva TM4C123GH6pm.ccxml or EPD_Extension_Board_TM4C123.ccxml
At “Start” it allows me to browse and point to an *.out file, usually in an Output folder named “EK-TM4C123GXL.out” to flash
I think you’re ok here.
Note when I am asked to ID my device the pull down choices sometimes refer to the board, EK-TM4C123GXL, and sometimes the Processor itself Tiva TM4C123GH6PMI. I have never been able to find “PMI” so I have used “PM”, I am not sure how significant that is.
It erases the and tells me program loaded successfully
If I verify the image I get “Status: CORTEX_M4_0: Program verification successful for C:/Users/Dogan/Documents/EPD Extension Board Gen2 (EXT2)_v1.21/Output/out/EK-TM4C123GXL.OUT”
Is there another step I am missing in telling the TI+PDIExtension Board Stack?
I am not sure how the required *.ccxml or the *.out files originated and if they include the image data or are they incomplete or corrupt.
The word “Image” UniFlash uses I assume is a file or like “sketch” in Arduino and does not refer to jpg, bmp PDI uses to convert into an *.epd EPaper display or *.c or *.h hexadecimal files they have used before.
This is my second TM4C1233GXL to rule out mechanical defects. I have ordered another Pervasive board and the two other Launch Pads they recommend MSP-EXP432P401r and MSP-EXP430F5529LP to try again. Any ideas would be appriciated