This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS3137: UART bootloader CMD

Part Number: TMS570LS3137


Tool/software: Code Composer Studio

I download an APP bin  file through UART Bootloader for Hercules TMS570LS31x Microcontroller to the TMS570LS3137 HDK.How to change the CMD file of the bootloader and the app?In the  bl_config.h we can see "#define APP_START_ADDRESS      0x00020000"

the bootloader CMD:


MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH_API (RX) : origin=0x00000020 length=0x000014E0
FLASH0 (RX) : origin=0x00001500 length=0x002FEB00 //LS31x and RM48 Flash size is 0x300000
STACK (RW) : origin=0x08000000 length=0x00002000
SRAM (RW) : origin=0x08002000 length=0x0002D000

}
SECTIONS
{
.intvecs : {} > VECTORS
flashAPI :
{
Fapi_UserDefinedFunctions.obj (.text)
bl_flash.obj (.text)
--library=..\lib\F021_API_CortexR4_BE.lib (.text)
} load = FLASH_API, run = SRAM, LOAD_START(api_load), RUN_START(api_run), SIZE(api_size)

.text > FLASH0
.const > FLASH0
.cinit > FLASH0
.pinit > FLASH0
.data > SRAM
.bss > SRAM
}

the app CMD:

/*----------------------------------------------------------------------------*/
/* Linker Settings */

--retain="*(.intvecs)"

/* USER CODE BEGIN (1) */
/* USER CODE END */

/*----------------------------------------------------------------------------*/
/* Memory Map */

MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x0017FFE0
FLASH1 (RX) : origin=0x00180000 length=0x00180000
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0003EB00

/* USER CODE BEGIN (2) */
/* USER CODE END */
}

/* USER CODE BEGIN (3) */
/* USER CODE END */


/*----------------------------------------------------------------------------*/
/* Section Configuration */

SECTIONS
{
.intvecs : {} > VECTORS
.text : {} > FLASH0 | FLASH1
.const : {} > FLASH0 | FLASH1
.cinit : {} > FLASH0 | FLASH1
.pinit : {} > FLASH0 | FLASH1
.bss : {} > RAM
.data : {} > RAM
.sysmem : {} > RAM

/* USER CODE BEGIN (4) */
/* USER CODE END */
}

I changed the two CMD files as follows:

But the app doesn't run and the LED D1 on the HDK brights out.It seems that an error occurs.

the changed bootloader CMD:

--retain="*(.intvecs)"


MEMORY
{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH_API (RX) : origin=0x00000020 length=0x000014E0
FLASH0 (RX) : origin=0x00001500 length=0x0001EB00 //LS31x and RM48 Flash size is 0x300000
FLASH1 (RX) : origin=0x00020000 length=0x00180000
SRAM (RW) : origin=0x08002000 length=0x0002D000
STACK (RW) : origin=0x08000000 length=0x00002000
}
SECTIONS
{
.intvecs : {} > VECTORS
flashAPI :
{
Fapi_UserDefinedFunctions.obj (.text)
bl_flash.obj (.text)
--library=..\lib\F021_API_CortexR4_BE.lib (.text)
} load = FLASH_API, run = SRAM, LOAD_START(api_load), RUN_START(api_run), SIZE(api_size)

.text > FLASH0
.const > FLASH0
.cinit > FLASH0
.pinit > FLASH0
.data > SRAM
.bss > SRAM
}

the changed app CMD:

/*----------------------------------------------------------------------------*/
/* Linker Settings */

--retain="*(.intvecs)"

/* USER CODE BEGIN (1) */
/* USER CODE END */

/*----------------------------------------------------------------------------*/
/* Memory Map */

MEMORY
{
VECTORS (X) : origin=0x00020000 length=0x00000020
//FLASH0 (RX) : origin=0x00000020 length=0x0017FFE0
FLASH1 (RX) : origin=0x00020020 length=0x0017FFE0
STACKS (RW) : origin=0x08030000 length=0x00001500
RAM (RW) : origin=0x08031500 length=0x0003EB00

/* USER CODE BEGIN (2) */
/* USER CODE END */
}

/* USER CODE BEGIN (3) */
/* USER CODE END */


/*----------------------------------------------------------------------------*/
/* Section Configuration */

SECTIONS
{
.intvecs : {} > VECTORS
.text : {} > FLASH1
.const : {} > FLASH1
.cinit : {} > FLASH1
.pinit : {} > FLASH1
.bss : {} > RAM
.data : {} > RAM
.sysmem : {} > RAM

/* USER CODE BEGIN (4) */
/* USER CODE END */
}