Part Number: DK-TM4C129X
Hi,
I am trying to read temperature values form TM100 temp sensor available in the Tiva C series evaluation board....
When I try to single step through code I get correct values for temp(3....when I try to run the code I get inconsistent values (even negative temp values) ..... What is the reason for this....
I am attaching the C code...
//*****************************************************************************
//
// slave_receive_int.c - Example demonstrating a simple I2C master message
// transmission using a slave interrupt when data is
// received.
//
// Copyright (c) 2010-2013 Texas Instruments Incorporated. All rights reserved.
// Software License Agreement
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
//
// This is part of revision 2.0.1.11577 of the Tiva Firmware Development Package.
//
//*****************************************************************************
#define TARGET_IS_SNOWFLAKE_RA0 // part no specifies 3 added to define silicon version
// DID0 reg value is 0x100A0002, signifies Snow flake class device version
//Die revision is A2 part revision 3
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_i2c.h"
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_types.h"
#include "driverlib/gpio.h"
#include "driverlib/i2c.h"
#include "driverlib/interrupt.h"
#include "driverlib/pin_map.h"
#include "driverlib/sysctl.h"
#include "driverlib/uart.h"
#include "utils/uartstdio.h"
//*****************************************************************************
//
//! \addtogroup i2c_examples_list
//! <h1>Slave Receive Interrupt (slave_receive_int)</h1>
//!
//! This example shows how to configure a receive interrupt on the slave
//! module. This includes setting up the I2C0 module for loopback mode as well
//! as configuring the master and slave modules. Loopback mode internally
//! connects the master and slave data and clock lines together. The address
//! of the slave module is set to a value so it can receive data from the
//! master.
//!
//! This example uses the following peripherals and I/O signals. You must
//! review these and change as needed for your own board:
//! - I2C0 peripheral
//! - GPIO Port B peripheral (for I2C0 pins)
//! - I2C0SCL - PB2
//! - I2C0SDA - PB3
//!
//! The following UART signals are configured only for displaying console
//! messages for this example. These are not required for operation of I2C.
//! - UART0 peripheral
//! - GPIO Port A peripheral (for UART0 pins)
//! - UART0RX - PA0
//! - UART0TX - PA1
//!
//! This example uses the following interrupt handlers. To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - INT_I2C0 - I2C0SlaveIntHandler
//
//*****************************************************************************
#define TempSensor_SlaveAddr 0x4A
#define Config_Reg 0x01
#define Temp_reg 0x00
#define SD_Configreg 0x01
//*****************************************************************************
//
// Set the address for slave module. This is a 7-bit address sent in the
// following format:
// [A6:A5:A4:A3:A2:A1:A0:RS]
//
// A zero in the R/S position of the first byte means that the master
// transmits (sends) data to the selected slave, and a one in this position
// means that the master receives data from the slave.
//
//*****************************************************************************
#define SLAVE_ADDRESS 0x4A // slave addr for temp sensor
//*****************************************************************************
//
// Global variable to hold the I2C data that has been received.
//
//*****************************************************************************
static uint32_t g_ui32DataRx;
//*****************************************************************************
//
// This is a flag that gets set in the interrupt handler to indicate that an
// interrupt occurred.
//
//*****************************************************************************
static bool g_bIntFlag = false;
//*****************************************************************************
//
// This function sets up UART0 to be used for a console to display information
// as the example is running.
//
//*****************************************************************************
void
InitConsole(void)
{
//
// Enable GPIO port A which is used for UART0 pins.
// TODO: change this to whichever GPIO port you are using.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOA);
//
// Configure the pin muxing for UART0 functions on port A0 and A1.
// This step is not necessary if your part does not support pin muxing.
// TODO: change this to select the port/pin you are using.
//
GPIOPinConfigure(GPIO_PA0_U0RX);
GPIOPinConfigure(GPIO_PA1_U0TX);
//
// Enable UART0 so that we can configure the clock.
//
SysCtlPeripheralEnable(SYSCTL_PERIPH_UART0);
//
// Use the internal 16MHz oscillator as the UART clock source.
//
UARTClockSourceSet(UART0_BASE, UART_CLOCK_PIOSC);
//
// Select the alternate (UART) function for these pins.
// TODO: change this to select the port/pin you are using.
//
GPIOPinTypeUART(GPIO_PORTA_BASE, GPIO_PIN_0 | GPIO_PIN_1);
//
// Initialize the UART for console I/O.
//
UARTStdioConfig(0, 115200, 16000000);
}
//*****************************************************************************
//
// The interrupt handler for the for I2C0 data slave interrupt.
//
//*****************************************************************************
void
I2C6MasterIntHandler(void)
{
//
// Clear the I2C0 interrupt flag.
//
I2CMasterIntClear(I2C6_BASE);
//
// Read the data from the slave.
//
g_ui32DataRx = I2CMasterDataGet(I2C6_BASE);
//
// Set a flag to indicate that the interrupt occurred.
//
g_bIntFlag = true;
}
//*****************************************************************************
//
// Configure the I2C0 master and slave and connect them using loopback mode.
//
//*****************************************************************************
int
main(void)
{
uint32_t ui32DataTx;
volatile uint32_t pui32DataRx;
uint32_t g_ui32SysClock; // acquire sysclk value
bool busyFlag = false;
//
g_ui32SysClock = SysCtlClockFreqSet((SYSCTL_OSC_MAIN | SYSCTL_XTAL_25MHZ | SYSCTL_USE_PLL | SYSCTL_CFG_VCO_480),
120000000);// changing to 25Mhz external crystal // Sysclk defined for 120Mhz
SysCtlPeripheralEnable(SYSCTL_PERIPH_I2C6);
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOB);
GPIOPinConfigure(GPIO_PB6_I2C6SCL); // pin mux
GPIOPinConfigure(GPIO_PB7_I2C6SDA); // pin mux
GPIOPinTypeI2C(GPIO_PORTB_BASE, GPIO_PIN_7);// Configures pin for use as SDA
GPIOPinTypeI2CSCL (GPIO_PORTB_BASE, GPIO_PIN_6);// Configures pin for use as SCL
I2CMasterInitExpClk(I2C6_BASE, g_ui32SysClock, true); // 400kbps
I2CMasterEnable(I2C6_BASE);
I2CMasterSlaveAddrSet(I2C6_BASE, TempSensor_SlaveAddr, false); //write
//
InitConsole(); // UART initialization
UARTprintf("I2C Mater Interrupt Example ->");
// Place the data to be sent in the data register.
I2CMasterDataPut(I2C6_BASE, Config_Reg);
I2CMasterControl(I2C6_BASE, I2C_MASTER_CMD_SINGLE_SEND); // send pointer addr
while(I2CMasterBusy(I2C6_BASE)) continue;
//Print
UARTprintf("\n Send Control reg addr!\n");
// read config reg
I2CMasterSlaveAddrSet(I2C6_BASE, TempSensor_SlaveAddr, true); // Config for read
I2CMasterControl(I2C6_BASE, I2C_MASTER_CMD_SINGLE_RECEIVE);
while(I2CMasterBusy(I2C6_BASE)) continue;
pui32DataRx = I2CMasterDataGet(I2C6_BASE);
// write to pointer reg for temp reg
I2CMasterSlaveAddrSet(I2C6_BASE, TempSensor_SlaveAddr, false); //Config for write
I2CMasterDataPut(I2C6_BASE, Temp_reg);
I2CMasterControl(I2C6_BASE, I2C_MASTER_CMD_SINGLE_SEND); // points to temp register
while(I2CMasterBusy(I2C6_BASE)) continue;
//read ist byte
I2CMasterSlaveAddrSet(I2C6_BASE, TempSensor_SlaveAddr, true); // Config for read
I2CMasterControl(I2C6_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
while(I2CMasterBusy(I2C6_BASE)) continue;
pui32DataRx = I2CMasterDataGet(I2C6_BASE);
pui32DataRx = pui32DataRx <<8;
// read second byte
I2CMasterControl(I2C6_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
while(I2CMasterBusy(I2C6_BASE)) continue;
pui32DataRx |= I2CMasterDataGet(I2C6_BASE);
pui32DataRx = pui32DataRx >>4;
UARTprintf(" 1st Reading :'%d' \n\n", pui32DataRx); // ist temperaure read
//
// I2CMasterSlaveAddrSet(I2C6_BASE, TempSensor_SlaveAddr, true); // Config for read
I2CMasterControl(I2C6_BASE, I2C_MASTER_CMD_BURST_RECEIVE_START);
while(I2CMasterBusy(I2C6_BASE)) continue;
pui32DataRx = I2CMasterDataGet(I2C6_BASE);
pui32DataRx = pui32DataRx <<8;
I2CMasterControl(I2C6_BASE, I2C_MASTER_CMD_BURST_RECEIVE_FINISH);
while(I2CMasterBusy(I2C6_BASE)) continue;
pui32DataRx |= I2CMasterDataGet(I2C6_BASE);
pui32DataRx = pui32DataRx >>4;
/* while(!(I2CMasterBusy(I2C6_BASE)))
{}*/
UARTprintf(" 2nd Reading:'%d' \n\n", pui32DataRx); // 2nd temp read
//
// Loop forever.
//
while(1)
{
}
}