This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
I am having a hard time using the ROM_ functions. I keep getting unresolved symbol errors. I have gone as far as copying the file rom.h into my project directory and have added theline
#include "rom.h"
I believe the compiler cant find the file and the symbols but can not figure out why. I have a number of funcs define in driverlib that all work as planned. It just seems rom.h doesnt want to cooperate.
any sugestions would be greatly appreciated.
Thanks
Pat
As explained in the Direct ROM Calls section of the TivaWare™ Peripheral Driver Library USER’S GUIDE:patrick murphy said:I am having a hard time using the ROM_ functions. I keep getting unresolved symbol errors.
Where one of the TARGET_IS_* macros defines the type of device.The device on which the application is run must be defined using a preprocessor symbol, which can be done either within the source code or in the project that builds the application. The latter is more flexible if code is shared between projects.
Without a valid TARGET_IS_* macro defined before including rom.h you end up with unresolved symbol errors.
Hello,
here are the unresolved symbols
ROM_SysCtlClockGet ./simple_rx_swc.obj
ROM_SysTickEnable ./simple_rx_swc.obj
ROM_SysTickIntEnable ./simple_rx_swc.obj
ROM_SysTickPeriodSet ./simple_rx_swc.obj
But, I went back to an old project that has ROM functions that work and searched for the TARGET_IS directive and found it only in a file in the project directory called //debug/drivers/subdir_rules.mk.
this same file in the current project does not have that directive. This file subdir_rules.mk is automatically generated. How is this file generated? From what info? I fairly certain that the new project
(where ROM doesnt work) was set up the same way as the old project( where ROM does work).
Thanks For the Help