Part Number: EK-TM4C1294XL
Hi,
I'm working on a Tiva-C TM4C1294XL board and I'm trying to send UDP packet to a computer. I just need to send data and I never need the computer to answer the board. I modified the enet_lwip example and even I can get an IP and ping the board, I'm not able to send any UDP packet. My first attempt is using a loop with udp_send() in it. I found on other post that normally udp_send() should be called from the ethernet handler. However I saw that it can work a time as in this post : 
With this code, I'm able to get the link, to get an ip and the board answer to the ping (so it is able to send data). However I'm not able to send any UDP packet and I don't know why. Ok as I wrote I know that normally the udp_send() must be used in the handler but it should at least send some udp datagram.
Do I need the udp_init() function ?
Do I need to free the pbuf ?
Do I need anything else just to send one datagram ?
int main(void)
{
struct udp_pcb * pcb;
BoardInit(); // Initialize the board.
ConsComInit(); // Initialize the communication with the computer via UART0.
PinoutSet(true, false); // Configure the device pins.
EthInit(); // Initialize the Ethernet port.
SysTickInit(); // Enable the System Timer
pcb = UdpInit(srv_ip , srv_port); // Initialize the UDP connection with remote server (same code than LocatorInit but return the PCB).
//Print relevant information to check if UdpInit is ok ---> the pcb is correctly configured
UARTprintf("\nLocal ip address should be any : ");
DisplayIPAddress(pcb->local_ip.addr);
UARTprintf("\nLocal port : %3d\n", pcb->local_port);
UARTprintf("Remote ip address : ");
DisplayIPAddress(pcb->remote_ip.addr);
UARTprintf("\nRemote port : %3d\n", pcb->remote_port);
struct pbuf * pb;
char str[512]="Test Veoware";
pb = pbuf_alloc(PBUF_TRANSPORT, 512, PBUF_REF);
pb->payload = str;
pb->len = pb->tot_len = 512;
while(1){ // I just try to send continuously the same info just to see if packet is sent.
udp_send(pcb, pb);
}
//Setup the device locator service.
//LocatorInit();
//LocatorMACAddrSet(pui8MACArray);
//LocatorAppTitleSet("EK-TM4C1294XL enet_io");
//UARTprintf("%d.",pui8MACArray );
//httpd_init();
// Set the interrupt priorities. We set the SysTick interrupt to a higher
// priority than the Ethernet interrupt to ensure that the file system
// tick is processed if SysTick occurs while the Ethernet handler is being
// processed. This is very likely since all the TCP/IP and HTTP work is
// done in the context of the Ethernet interrupt.
MAP_IntPrioritySet(INT_EMAC0, ETHERNET_INT_PRIORITY);
MAP_IntPrioritySet(FAULT_SYSTICK, SYSTICK_INT_PRIORITY);
// Loop forever. All the work is done in interrupt handlers.
while(1)
{
}
}