This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS3137: TMS570LS3137

Part Number: TMS570LS3137

Tool/software: Code Composer Studio

Hi,

I am working on a code which was built with the CCS v.5.5 and the customized linker_file is used. currently I am using is  CCS v.6.0.1 and same linker_file I am using here.

For which warnings are generating as below

" warning #10068-D: no matching section"

I have cross verified to check syntax errors for the linker_file. there are no syntax errors

can I get some suggestion to solve this issue,

With Regards

Shankar