Part Number: TM4C1290NCPDT
Other Parts Discussed in Thread: TM4C1294NCPDT
Team,
From our Tiva customer:
-----
In the Tiva data sheet (DS-TM4C1290NCPDT-15863.2734, SPMS429B), Figure 10.1 (page 725 in my version) is a diagram of the Digital I/O pads.
I need closer view of what is inside the “Digital I/O Pad” box on the right. In particular, I’m trying to understand the connections between the actual pin, at what point the “input pad” is sampling, and the output pin.
The underlying objective is to monitor an output (ideally the actual physical pin) with the input on the same I/O channel, to detect when some sort of hardware failure is active (external PC trace stuck high, internal transistor driver failure, etc.).
Can you find info that would help?
-----
Thanks for your help in advance!!
-CY