Part Number: TMS570LS0714
Dear All
We are using tms570ls0714 to do a safety critical project, which aimed to get the SIL4 of EN50128.
We decided to use the ECC functions. But the assessors were astonished when they hear that ECC can change the data and program on flash section.
We explained that when there is a single bit error, the cpu will correct that, and it will improve our safety level. But they don't agree, they think the program context can not be changed all the time.
They ask for the certificate of the ECC function to prove that ecc detection and correction logic is safe and reliable.
Can you guys offer me something related?
And another issue is that in the doc SPNU550A,you mentioned "
Safety Analysis Report Summary for TMS570LS12x and TMS570LS11x ARM?-Based Safety Critical Microcontrollers (SPNU530)
Detailed Safety Analysis Report for TMS570LS12x and TMS570LS11x ARM?-Based Safety Critical Microcontrollers (SPNU531) "
I cannot find these two docs anywhere. I'd like to have these two docs related to tms570ls0714 and 1227?
Thank you so much.
Best Regards
Leo