Part Number: RM46L852
We are currently selecting a microcontroller for an application which must be compliant with IEC 60730 Class C. Looking through the SafeTI pages, a number of C2000 family microcontrollers are recommended for IEC 60730 applications, however we have had difficulties in getting these to work with some of our tools due to the 16-bit minimum addressable unit.
The RM46 family looks like a good alternative from the specification with what appears to be many superior safety related features. However, this family seems to be recommended more for IEC 61508 applications. Is there any reason why the RM46 family would not be suitable for a 60730 application or why they are not suggested on the SafeTI-60730 page? Also, are there any plans to try to certify the Hercules hardware or safety diagnostic software libraries with TUV for IEC 60730 compliance if they haven't been already?