Hello all.
Dear Amit, Charles, Bob, Bruno, cb1 and all the other good-fellas here at the forum, I need-want-dream to RESURRECT the *** TI-59 LEGEND *** on a TM4C1294NCPDT module. According to my knowledge on TI-59 and the hardware printed material that I have since the TI59's era and also my current understanding of the TM4C1294NCPDT module I can assess that this is an achievable and worth trying effort.
WHY: I am convinced that TI-59 is/was a machine that one could use to study and learn assembly in a matter of days. The philosophy of this machine's programming schema was as close to the machine language as to that of a higher-level's logic programming language. As far as I'm aware of, no other computer / programming language combination was so successful in demonstrating the full operational and functional esoteric marvels of computers. I am convinced that such an effort could help many-many children & students to step into the computer's field very smoothly and also many other people of some age to realize the nature of how things evolve. It would also be a very good opportunity to demonstrate and teach to the more curious young minds how compilers work and what they actually do. [HP-41C could also be another good candidate for such a project but let's let another guy do this]
HOW: I assume that the creators of this TI-59 marvel are not any more around TI's HQ or even easy to locate. But the designs and the programming infrastructure manuals must surely be able to be found somewhere in the archives of TI. That given, I would be very pleased if a person from TI could come in contact with me to collaborate and assist me in gathering of the needed material. That's all I need. It would be of course one of a case if one of the principal designers of TI-59 could also be located and assist in providing valuable info.
The profits from such a project could be many for both TI and for Users & Customers of TI's products and for any one else directly or indirectly involved in the, or, with activities regarding the educational spectrum.
All the best,
John