Hello,
I'm attempting to debug a problem that seems to exist since Tivaware 2.1.3, although I've been doing the majority of my testing with Tivaware 2.1.4.178.
If I build the project against Tivaware 2.1.2.111 everything works as expected as far as USB insertion/removal is concerned. If I then rebuild against Tivaware 2.1.4.178 and flash that code onto the device, USB detection will work for a little while, but then something happens which breaks the insertion detection. After that happens I am unable to get the USB insertion detection working unless I revert back to Tivaware 2.1.2.111.