Part Number: TM4C123GH6PM
I am using the Tiva C LaunchPad and Kentec boosterpack. My original goal is to take readings from 2 ADC's, compare them, and flash an LED when I get a pin interrupt if ADC1>ADC2. I have that code and circuitry working fine.
Now I am moving on to trying to display values on the screen of each of the ACD's. I figured I'd start small and just try to get an image to show up on the Kentec screen while the rest of the circuit is functioning. After messing around for a while I finally got an image to pop up on the screen along with all the other parts of the program functioning properly. However, I discovered that I need to have the ADC sampling be <2 samples/second or the image will not load properly. As I increase the samples/second less and less of the image will load.
For the real screen I am just going to have basic text, buttons, and inputs. But I'm concerned that the processor might not be able to handle the screen as well as the functions I need it to do in order to do the "main" job of the controller.
Should this processor be able to handle both a small screen (maybe up to 5") as well as basic motor control with 10 samples/sec and outputting a signal at up to 120Hz?