Part Number: TMDXRM46HDK
Other Parts Discussed in Thread: RM46L852, HALCOGEN
Hello,
I have evaluated the RM46L852 with the Hercules RM4 MCU development kit (TMDXRM46HDK) and now want to build a PCB that incorporates the RM46L852 processor for safety functions following the IEC 61508 standard.
It is my understanding that the development kits are for test purposes only, so to actually use the RM46L852 for a safety function I will need to design my own PCB. With the Hercules RM4 MCU, it was easy to get the desired functionality up and running; however, designing a PCB from scratch adds a lot more complexity. I have not found much information on how to actually accomplish this.
Desired specs:
- The PCB needs to connect to magnetic safety switches to detect if they are open or closed.
- The PCB needs to communicate through USB or UART RS232.
- I intend to program the board using an external XDS100v2 Emulator connected to pins
Questions:
When designing my PCB, how do I configure the board to program the RM46L852 processor? Will I be able to use CCS and HALCoGen on this PCB? Additionally, how would I configure the board to allow UART or USB communication? It seems that on HDK board, the UART (SCI) only goes through the JTAG connection. Is there a way to enable SCI communication without having the JTAG emulator present?
Also, to ensure that IEC 61508, I know that I will need to include a TPS65381 voltage monitor for the RM46L852, but what other considerations do i need to take into account to ensure the PCB complies with safety standards?
Thanks,
Chris