Part Number: TM4C1231E6PM
Other Parts Discussed in Thread: EK-TM4C123GXL
Hi,
one of my customers wants to estimate the ambient temperature using the internal temp channel of the ADC. We are aware that the accuracy is specified with +/-5°C.
When measuring the temp sensor, we get a reading that is within this accuracy specification. We need guidance on the influence of the PE3 pin on the temp sensor reading. When the voltage of this pin changes, the reading is immediately influenced. We couldn't find any description of this behaviour nor any errata that seems to cover this.
Just to be sure that this behavior is not related to customer's application, I put together a example project running on our EK-TM4C123GXL. Please find this project attached (using Tivaware 2.1.4.178)TM4C123GH6_temp_sensor.zip. I tried with both PE3 enabled as well as disabled. To vary the voltage at PE3, I connected a jump wire between this pin and either +3.3V or GND. Result of the measurements:
As you can see, the reading is lower when PE3 is connected to GND and increases when PE3 is connected to +3.3V.
What is the reason for this behavior? How to avoid it?
Best regards,
Phil