Part Number: EK-TM4C1294XL
Tool/software: TI-RTOS
Hi,
I have tried using the http server example downloaded from this wiki page on EK-TM4C1294XL board.
The HTML files are being properly rendered and the CGI functions are being invoked without any issue.
However, the delay for a GET response is around 10-20 ms for initial requests. But, after 10 to 15 continuous calls the delay is peaking to 3000ms for most of the calls thereafter.
I have tested the delay using a REST client (Postman).
And after the http server is standby for about 20 minutes, I am not getting any response and had to reset the board.
I have tried this without any modifications to the code in the example.
Please help resolve the issue.
Thanks,
Ayyappa