Part Number: EK-TM4C1294XL
Tool/software: Code Composer Studio
I have to make a program for the ADC from the TIVA, but I can't use libraries other than stdbool and stdint. Here's my code, and when I try to debug it, it stucks when I want to check if the conversion has finished.
The program is intended for using the temperature Sensor in the Microprocessor.
#include <stdbool.h>
#include <stdint.h>
#define SYSCTL_RCGCGPIO_R (*((volatile uint32_t *)0x400FE608))
#define SYSCTL_PRGPIO_R (*((volatile uint32_t *)0x400FEA08))
#define SYSCTL_RCGCADC_R (*((volatile uint32_t *)0x400FE638))
#define SYSCTL_PRADC_R (*((volatile uint32_t *)0x400FEA38))
#define ADC0_PC_R (*((volatile uint32_t *)0x40038FC4))
#define ADC0_SSPRI_R (*((volatile uint32_t *)0x40038020))
#define ADC0_ACTSS_R (*((volatile uint32_t *)0x40038000))
#define ADC0_EMUX_R (*((volatile uint32_t *)0x40038014))
#define ADC0_SSEMUX3_R (*((volatile uint32_t *)0x400380B8))
#define ADC0_SSMUX3_R (*((volatile uint32_t *)0x400380A0))
#define ADC0_SSCTL3_R (*((volatile uint32_t *)0x400380A4))
#define ADC0_IM_R (*((volatile uint32_t *)0x40038008))
#define ADC0_ACTSS_R (*((volatile uint32_t *)0x40038000))
#define ADC0_ISC_R (*((volatile uint32_t *)0x4003800C))
#define ADC0_PSSI_R (*((volatile uint32_t *)0x40038028))
#define ADC0_RIS_R (*((volatile uint32_t *)0x40038004))
#define ADC0_SSFIFO3_R (*((volatile uint32_t *)0x400380A8))
void main(void){
SYSCTL_RCGCADC_R = 0x01; // Clock Enable for ADC
while((SYSCTL_PRADC_R&0x01)==0); // Delay for the clock enable
ADC0_PC_R = 0x01; // 125Ksamp/s
ADC0_SSPRI_R = 0x0123; // SS3 with the top priority
ADC0_ACTSS_R = 0x0000; // Disables SS3 before the configuration
ADC0_EMUX_R = 0x0000; // Software enable for the sampling
ADC0_SSEMUX3_R = 0x00; // Pins AIn(15:0)
ADC0_SSMUX3_R = (ADC0_SSMUX3_R & 0xFFFFFFF0) + 9; // AIN9 Channel
ADC0_SSCTL3_R = 0x000E; // Enabling the Temperature Sensor, INR3 Enable, End Sequence; No diferencial mode
ADC0_IM_R = 0x0000; // Disables SS3 interruptions
ADC0_ACTSS_R |= 0x0008; // Enables SS3
ADC0_ISC_R = 0x0008;//Clears Flags
while{
uint32_t adc_result;
float TEMP;
ADC0_PSSI_R = 0x0008; // Starts Conversion
while ((ADC0_RIS_R & 0x08)==0); // ALWAYS STUCK HERE
adc_result = (ADC0_SSFIFO3_R & 0xFFF);// Saves the conversion result to adc_result
ADC0_ISC_R = 0x0008; // Clears flags
TEMP = 147.5 - ((75 * (3.3) * adc_result)/ 4096);
}
}