Part Number: TIDA-00203
Tool/software: Code Composer Studio
We have been running the CAN to Ethernet demo successfully on the TIDA-00203 web site. It always worked for us. We can ping the board at 169.254.254.255 (default IP for demo) and run the CAN demo through either a direct connection with a laptop (Gigabit NIC) performing the telnet successfully OR through a Fast Ethernet 10/100 switch. When we put a Gigabit switch between the TIDA-00203 and the laptop we cannot ping the TIDA-00203 board anymore and the demo does not work! We tried 2 different Gigabit unmanaged switches and we cannot ping the TIDA-00203 through a Gigabit switch. Any ideas on why this is and is there a software setting in the code that we can make to fix this? The TIDA-00203 must have a problem negotiating with the GigE Switch (even though the switches we tried support 100 Mb Ethernet and give us a 100 Mb link light).
Regards,
Todd