Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
Hello,
I am using a TMS570LS1224 board and CCS version 7.
I am trying to run a simple program that doesn't do anything on the board in debug mode. The code compiles and runs, but I'm noticing a problem when I search "main" in the memory browser under 32-Bit Hex - TI Style. The first couple of sections in hexadecimal code, 0x00000000 through 0x00000020, remain uninitialized. It appears like this:
0x00000000 FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF
0x00000010 FFFFFFFF FFFFFFFF FFFFFFFF FFFFFFFF
This will cause problems in future code that I run on the board if I do not resolve it. I have traced the problem to the linker file, "TMS570LS122xFlashLnk.cmd". In the Section Configuration, there is a section called".intvecs" that is not currently pointing to any code files.
/*----------------------------------------------------------------------------*/
/* TMS570LS122xFlashLnk.cmd */
/* */
/* (c) Texas Instruments 2011, All rights reserved. */
/* */
/* USER CODE BEGIN (0) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Linker Settings */
--retain="*(.intvecs)"
/*----------------------------------------------------------------------------*/
/* Memory Map */
MEMORY{
VECTORS (X) : origin=0x00000000 length=0x00000020
FLASH0 (RX) : origin=0x00000020 length=0x0013FFE0
STACKS (RW) : origin=0x08000000 length=0x00001300
RAM (RW) : origin=0x08001300 length=0x0002ED00
}
/*----------------------------------------------------------------------------*/
/* Section Configuration */
SECTIONS{
.intvecs : {} > VECTORS
.text : {} > FLASH0
.const : {} > FLASH0
.cinit : {} > FLASH0
.pinit : {} > FLASH0
.bss : {} > RAM
.data : {} > RAM
}
/*----------------------------------------------------------------------------*/
.intvecs appears black in color, while the other sections are colored purple, this further tells me that something is wrong with it. I have been looking through my computer's files (Macintosh HD > Applications > ti > ccsv7 > ccs_base > arm) for files that contain the code for those eight hexadecimal lines, but I cannot find anything that helps.
Looking through the online manuals and reference guides for the board, I have found that .intvecs should contain something like this:
"; interrupt vectors
resetEntry:
0x00 b _c_int00
undefEntry:
0x04 b undefEntry
svcEntry:
0x08 b svcEntry
prefetchEntry:
0x0C b prefetchEntry 0x10 b _dabort 0x14 b phantomInterrupt 0x18 ldr pc,[pc,#-0x1b0] 0x1C ldr pc,[pc,#-0x1b0]"
I have been looking for a .c file that contains these, but I have yet to find one. Where can I find the file that contains what I need?