Part Number: TMS570LC4357
Hi,
We plan to use the EMIF to communicate with an external device (FPGA) for accessing its registers. As far as I know, from the EMIF point of view this will be managed as asynchronous accesses.
I am looking to identify the maximum VCLK3 frequency that I can setup:
- Is it 150MHz as indicated in chapter "6.6.2 Clock domains" of the TMS570LC4357 datasheet (see table 5-2. Clock Domain Timing Specification")?
- Is it 100MHz due to the "tc(CLK)" minimum value of 10ns found in "Table 6-38. EMIF Synchronous Memory Switching Characteristics"? >> Then, is this constraint on tc(CLK) only applicable for synchronous accesses?
From a FPGA designer in our team, it looks like the it would be interesting to use the EMIF clock signal (if available), even for asynchronous accesses:
- Do you confirm that the EMIF_CLK signal is output at any time, regardless of the EMIF configuration?
- Does this pin can output a signal of 150MHz if VCLK3 can be configured at 150MHz?
Best regards,
Gael