Part Number: TMS570LS3137
Hello,
Currently, I am designing a PCB which will include the TMS570. I need to have a debugging connection, but due tight size constraints, I am not going to be able to use the 20 pin header used in the TMS570 development board. I have been looking for other options that I could use, but I have not clear if all of the are suitable for the TMS570.
-Which is the smaller connector able to work with the TMS570?
- Could I use a debugger made for the standard 20 pin header and use an adaptor for using a smaller one? For example, could I use this debugger (www.ti.com/.../TMDSEMU100v2U-20T ) and use an adapter for this header cfile24.uf.tistory.com/.../140CEE1E4CE1F5BA320197
Regards,
Ander