Part Number: RM46L430
Other Parts Discussed in Thread: HALCOGEN
The RM46 Reference Manual SPNU514B–April 2015, section 10.4.6 Trimming the HF LPO Oscillator says:
'During device test, a trim value is written into the one-time programmable section of the flash memory (OTP), address 0xF008_01B4.'
It also says:
'When trimming the HF LPO, it is recommended to step the trim value so as not to make a large change to any TRIM setting.'
The HalCoGen example code:
- Checks to see if the 16-bit trim value is '0xFFFF', in which case it does not apply it.
- Does not change the trim value in steps.
I cannot find any information regarding the LPO trim in the SafeTI Library / Safety Manual or anything relevant in a previous community post, so my questions are:
- Is there a requirement to use a trim value of zero if the OTP read is 0xFFFF?
- What is the recomended maximum step?
- What is the recomended pause between steps?
- Where can I find the documents that specify these requirements?