Hello
My customer is siing problems with the TM4C1294NCPDT as soon as the environment gets close to 95% humidity.
Then either the CANBUS interface drops out or the status LED (connect to pin 63) connected stops pulsing as it was previously. Although they can still communicate via the UART at this temperature.
Do you know of any known issues or problems that might cause this ?
They also ask if we could indicate why the MSL is only up to 60% RH? Is there a reason it was tested to a higher level?
Best Regards
Bob Bacon