Tool/software: Code Composer Studio
Hi,
I am trying to get board that we build to work in ULPI host mode, the ulpi chip is USB3320 and I have it configured for internal clock source.
the target is a hub.....
I can read and write the registers with no errors ever , but nothing is going on with the bus.
The USB0 DEV_CTL register indicates that it is in device mode and I cannot get it to go to host mode.
I had this board running on USB full speed with internal usb connection and hub with no issues.
The board was designed to allow for either internal or external usb, but one or the other only.