Part Number: TM4C123GH6PM
Does TM4C123GH6PMI have LIN support.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The TM4C123GH6PM does not have all of the built in LIN support like the safety microcontroller RM41L232, or the rest of that family, but you can do LIN communication using the UART on the TM4C123GH6PM. The break generation and detection, as well as the 16 byte transmit and receive FIFO help support LIN communication. You will need to rely on the CPU to calculate and check checksums and identify slave ID's (if using as a LIN slave node).
My Dad - and my "status (1LT) w/in the US Army" - earned such salutation. Not so much, today.
Such MCUs exist - you were advised to "contact via PM" through the forum. (you need to set this w/in your forum registration page)
It is NOT good form to identify (others') devices from w/in this vendor's (public) forum... (PM method avoids such breach)
Bob Crosby said:The safety microcontroller
Might it be noted that "LIN" is specifically aimed towards, "Non-Safety and/or Critical" Applications - while aiming for "Low Cost?"
First post in response noted such...