Part Number: TM4C123GH6PM
Tool/software: TI-RTOS
I tried to use Uart to connect to Putty, I use CCS7.0.0
the console shows the following error
"../EK_TM4C123GXL.cmd", line 66: error #10099-D: program will not fit into available memory. run placement with alignment fails for section ".vtable" size 0x26c , overlaps with ".vecs", size 0x360 (page 0)
error #10010: errors encountered during linking; "P2_Putty.out" not built
I think there's some problem for my header file, if I include the #include "inc/tm4c123gh6pm.h", it will shows 72 warnings.
please help me to check where's the problem, thanks!
The project are attached below