Part Number: TM4C123GH6PM
Hi i am implementing the usb mass storage device, when i connect my usb cable connected to TM4C123GH6PM to windows 10 i get the device displayed and i get and device descriptor error, i am using the example dk-tm4c123g/usb_dev_msc and configured the pins according to my custom board. though my serial device is working fine in both windows as well as linux.
while i was debugging in linux i can observe i am not getting any usb device but when i disconnect the device interrupt callback function gets called but when i connect the device callback function is not called.