Other Parts Discussed in Thread: OMAP-L137, HALCOGEN, SYSBIOS
I have several question regarding the TMS570 development board which I purchased from TI.
1. According to the Keil website, the development kit comes preprogrammed with the board confidence test and demo application which is available on the DVD that comes in the kit. Is this application available to those of us that purchased the board from TI instead of Keil? This would be a good example of how to interface to the touch screen. If not, is there any thing else that can help explain how to use the touchscreen?
2. Are there any example programs or documentation on how to use the ethernet and usb ports which I believe are handled by an omap device on the cpu board.
3. Are there any example programs or documentation on how to use the FRAM device or SD card.
The TMS570 Safety MCU Demos program that comes with the TI kit does not address any of these needs.
-Walt