Part Number: EK-TM4C123GXL
Tool/software: Code Composer Studio
Hello all,
Now, that's a more complex problem I have (I think), I spent hours trying to make ADC work, without success. I'm trying to read 7 values, on pins PE0 through PE4, PB4 and PB5. When I apply 3V3 on all pins, PE0 PE1 PE2 and PE3 are reading 3V3 normally, but the others fluctuate between 3V3 and random values. When I try to read some pin alone, all the pins fluctuate.
What I tried to do:
- Enable only ADC0, SS0
- Enable ADC0 and ADC1, both SS1
- Change the clock source from PIOSC to PLL (configuring to give 16MHz on both)
- Change TRIGGER_ALWAYS to TRIGGER_TIMER
- Trigger the ADC at low speed (1Hz)
- Comment out the ADCReferenceSet()
What I have enabled on my project:
- TIMER0,1,2,3,4,5
- WTIMER0,2
- WTIMER1 as edge capture pins PC6 PC7
- PWM0, pins PB7 PC5 PE5
- PWM1, pin PF1
- OUTPUT Pins PB2 PB3 PD0 PD1 PD2 PD3
- INPUT Pins PA2 PA3 PA4 PA5
- UART0 and PA0 PA1
- HIBERNATE RTC
- ADC0 Pins PE0 PE1 PE2 PE3
- ADC1 Pins PE4 PB4 PB5
Here is some sample code I'm using to config ADC:
inline void config_ADC0(void)
{
MAP_SysCtlPeripheralDisable(SYSCTL_PERIPH_ADC0);
MAP_SysCtlPeripheralReset(SYSCTL_PERIPH_ADC0);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC0);
while(!MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_ADC0));
MAP_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_0 | GPIO_PIN_1 | GPIO_PIN_2 | GPIO_PIN_3);
MAP_ADCReferenceSet(ADC0_BASE, ADC_REF_INT);
MAP_ADCSequenceConfigure(ADC0_BASE, 1, ADC_TRIGGER_TIMER, 0x00);
MAP_ADCSequenceStepConfigure(ADC0_BASE, 1, 0, ADC_CTL_CH0 | ADC_CTL_IE);
MAP_ADCSequenceStepConfigure(ADC0_BASE, 1, 1, ADC_CTL_CH1 | ADC_CTL_IE);
MAP_ADCSequenceStepConfigure(ADC0_BASE, 1, 2, ADC_CTL_CH2 | ADC_CTL_IE);
MAP_ADCSequenceStepConfigure(ADC0_BASE, 1, 3, ADC_CTL_CH3 | ADC_CTL_IE | ADC_CTL_END);
ADCClockConfigSet(ADC0_BASE, ADC_CLOCK_SRC_PLL | ADC_CLOCK_RATE_FULL, 25);
MAP_ADCHardwareOversampleConfigure(ADC0_BASE, 64);
MAP_ADCSequenceEnable(ADC0_BASE, 1);
MAP_IntDisable(INT_ADC0SS1);
MAP_ADCIntDisable(ADC0_BASE, 1);
MAP_IntPendClear(INT_ADC0SS1);
MAP_ADCIntClear(ADC0_BASE, 1);
MAP_IntPrioritySet(INT_ADC0SS1, 0x20);
MAP_IntEnable(INT_ADC0SS1);
MAP_ADCIntEnable(ADC0_BASE, 1);
}
inline void config_ADC1(void)
{
MAP_SysCtlPeripheralDisable(SYSCTL_PERIPH_ADC1);
MAP_SysCtlPeripheralReset(SYSCTL_PERIPH_ADC1);
MAP_SysCtlPeripheralEnable(SYSCTL_PERIPH_ADC1);
while(!MAP_SysCtlPeripheralReady(SYSCTL_PERIPH_ADC1));
MAP_GPIOPinTypeADC(GPIO_PORTE_BASE, GPIO_PIN_4);
MAP_GPIOPinTypeADC(GPIO_PORTB_BASE, GPIO_PIN_4 | GPIO_PIN_5);
MAP_ADCReferenceSet(ADC1_BASE, ADC_REF_INT);
MAP_ADCSequenceConfigure(ADC1_BASE, 1, ADC_TRIGGER_TIMER, 0x00);
MAP_ADCSequenceStepConfigure(ADC1_BASE, 1, 0, ADC_CTL_CH9 | ADC_CTL_IE);
MAP_ADCSequenceStepConfigure(ADC1_BASE, 1, 1, ADC_CTL_CH10 | ADC_CTL_IE);
MAP_ADCSequenceStepConfigure(ADC1_BASE, 1, 2, ADC_CTL_CH11 | ADC_CTL_IE | ADC_CTL_END);
ADCClockConfigSet(ADC1_BASE, ADC_CLOCK_SRC_PLL | ADC_CLOCK_RATE_FULL, 25);
MAP_ADCHardwareOversampleConfigure(ADC1_BASE, 64);
MAP_ADCSequenceEnable(ADC1_BASE, 1);
MAP_IntDisable(INT_ADC1SS1);
MAP_ADCIntDisable(ADC1_BASE, 1);
MAP_IntPendClear(INT_ADC1SS1);
MAP_ADCIntClear(ADC1_BASE, 1);
MAP_IntPrioritySet(INT_ADC1SS1, 0x20);
MAP_IntEnable(INT_ADC1SS1);
MAP_ADCIntEnable(ADC1_BASE, 1);
}
I have no idea what to do next. Suggestions?
Thanks!