Part Number: DK-TM4C129X
I would like to be able to adjust the time of occurrence of a DMA, relative to an external signal requesting it. Is it possible to connect that external signal to a GPTM CCP input and cause the timer to generate a uDMA trigger a configurable number of clock cycles after an edge on the external signal? What is the setup for this? Do you have example code?