Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C1294XL: MODBUS TCP

Part Number: EK-TM4C1294XL

Hello Everyone,

I am very new to this micro controller. This micro attracts me because it has MAC/PHY built in on the IC, so whenever I go to the production stage, I do not need to add external MAC/PHY chips.

I intend to use this MCU to collect and send the data to our main system which use MODBUS TCP as our communication protocol. I need to implement slave modbus tcp on the MCU. However, we do not want spend any effort to write our own modbus library.

So, is there any paid/free modbus library that I can test and use on this particular MCU.

Best Regards,

Yo Shua