Other Parts Discussed in Thread: HALCOGEN
Hi,
I am using on-chip CAN2 peripheral of the microcontroller for receiving the CAN data. I have configured messages from 49 to 64 for the reception with the CAN ID values from 0x00 to 0x0F. The mask for the all the CAN IDs is: 0x0000000F.
| Message box number | CAN Id | Mask |
| 49 | 0x00 | 0x0000000F |
| 50 | 0x01 | 0x0000000F |
| 51 | 0x02 | 0x0000000F |
| 52 | 0x03 | 0x0000000F |
| 53 | 0x04 | 0x0000000F |
| 54 | 0x05 | 0x0000000F |
| 55 | 0x06 | 0x0000000F |
| ... | ... | ... |
| 64 | 0x0F |
0x0000000F |
The configuration of the CAN messages is as shown in the above table. I receive all the CAN messages without any problem for more than 10 hours. All of a sudden, the controller stops receiving all CAN messages with messagebox number 49 (any message with last hex digit 0). The microcontroller does not trigger an interrupt for those messages. (the function can2HighLevelInterrupt() does not get called for the messages of messagebox number 49 anymore) All other CAN messages have no problem at all and trigger the ISR.
Do we have to implement any register bit clearing/setting in addition to the provided halcogen code? We are using HalCoGen version 04.06.00
We only use canGetData() as well as canGetID() so far.
Thanks & best regards,
Sreekanth challa
| Message box number | CAN Id | Mask |
| 49 | 0x00 | 0x0000000F |
| 50 | 0x01 | 0x0000000F |
| 51 | 0x02 | 0x0000000F |
| 52 | 0x03 | 0x0000000F |
| 53 | 0x04 | 0x0000000F |
| 54 | 0x05 | 0x0000000F |
| 55 | 0x06 | 0x0000000F |
| 56 | 0x07 | 0x0000000F |
| 57 | 0x08 |
0x0000000F |