This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GIODINA Inputs Only Read With Emulator (SD XDS510) Connected



I am seeing a difference in the ability to read the state of a GIO digital input when the TMS570LS20216ASPGE is running with  an emulator connected and when the part is running with the emulator in the disconnected state.  When the emulator is connected, the value of the port is correctly reported in the GIODINA register (i.e. I can see the bit corresponding to GIOA[5] change states 0 to 1 when I change the pin input value).  However when the emulator is disconnected, the bit for GIOA[5] is always reported as 0.

 

MEASUREMENT SETUP:

In all cases, I am using XCP protocol over FlexRay to monitor the values of the registers.

 

REGISTER CONFIGURATION VALUES:

GIODIRA = 0001 1011

GIODOUTA = 0001 0000

GIOEMUA = 0000 0000

GIODRA = 1000 0000

GIOPSLA = 0000 0000

GIOPULDISA = 1110 0000

PWRDWNSET1 = 0

PWRDWNSET2 = 0000 0000 0001 0000

PWRDWNSET3 = 0

 

How is the emulator impacting my ability to read a DIO pin?