Part Number: TM4C123GH6PM
Hi!,
It seems that Table 11-6 (on page 711) in the TM4C123GH6PM datasheet (DS-TM4C123GH6PM-15842.2741 SPMS376E) is incorrect in the Max Time Column. The times listed for pre-scale values of 0, 1 and 0xffff are correct, but the values other than those are incorrect. This can be seen as the values are increasing by a factor 2 at each step, while they should be increasing at increments of 53.687s .
How does this correction get propagated to the datasheet?
Thanks,
ed
--