Part Number: TM4C123GH6PM
I am debugging code that uses both the C Tiva Peripheral library and the MAP_xxx library calls.
My first call is
SysCtlClockSet(SYSCTL_SYSDIV_4 | SYSCTL_USE_PLL | SYSCTL_OSC_MAIN | SYSCTL_XTAL_16MHZ);
After this call is
s_ui32SysClock = MAP_SysCtlClockGet();
Debugging in assembly
LDR.N R0, PC, #0x94
R0:001000044
LDR R0, [R0]
R0:0xCDCDCDCD
When I look at memory 0x01000000 I see nothing but 0xCD bytes for all of memory.
Where has the ROM based Tiva peripheral library gone?
I have been working with this processor for months and never encountered this problem.
I am using the IAR IDE.
The version of Tiva peripheral library is 2.1.2.111