Part Number: TMS570LS2124
Hi,
One of my customers is using Flash bank 7 sector 2 for parameter storage. And they'd like to get a data abort error in case someone is reading from an erased flash location. But for bank 7 no data abort error is generated. When trying the same with and other bank, it's working fine.
EE_ALL1_OK is set to 0 and EE_EDACEN to a value other than 0101. With this I would expect to get the data abort error when accessing an erased flash location in bank 7.
Or is this not supported for bank 7, as the flash accesses are routed differently for this bank?
Thanks,
Robert