Part Number: TM4C1294NCPDT
Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
I am using TI-RTOS V2.16 for TM4C1294NCPDT microcontroller.
I am trying to use secute_iot project working on my application board. I have followed all steps to include wolfssl in to my project as shown in
http://processors.wiki.ti.com/index.php/Using_wolfSSL_with_TI-RTOS
My project grabs IP address from our network but then it crashes with task stack overflow . Please see the error below.
[CORTEX_M4_0] Using MAC address in flash
Starting BIOS
Service Status: DHCPC : Enabled : : 000
Service Status: DHCPC : Enabled : Running : 000
Welcome to the Crypto Connected LaunchPad's,
Secure Internet of Things Demo.
MAC Address: 001ab602a2c4
Network Added: If-1:10.40.149.61
Service Status: DHCPC : Enabled : Running : 017
ti.sysbios.knl.Task: line 373: E_stackOverflow: Task 0x20001548 stack overflow.
xdc.runtime.Error.raise: terminating execution
I also checked ROV and here is the result. It seems ShaTransform is over flowing which I believe declared in wolfssl.aem4f.
Please help.