Part Number: RM48L952
Other Parts Discussed in Thread: HALCOGEN
Tool/software: Code Composer Studio
I'm using Halcogen to generate code for CCS project. I choose the option RM48l950ZWT_FREERTOS and I try to add HET driver. the code was generate for HET the clock signal and output pin works just fine but I notice that het1LowLevelInterrupt in VIN RAM isn't generated in sys_vim.c file anymore. I need the notification to add some code of my own. if I choose the option without FREERTOS then the interrupt and notification code is generated but it is not there when I choose FREERTOS option. is this a bug or TI purposely remove HET notification when run with FREERTOS. I can't use vApplicationTickHook because this is too slow, I need some thing that run at 1usec period. is there a work around for this problem? I can try to add in the code manually but just wonder if there is some other setting that I might have missed. just don't want to have my manual code get wipe out the next time I decide to update tools in halcogen.
thanks